This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24450 Component Calculation Help

Other Parts Discussed in Thread: BQ24450

Hello,

I am planning on using the BQ24450 to charge two 12V 3.4Ah SLA batteries. When trying to calculate the component values Im having difficulty with the following equation:

Vboost = Vref × (RA + RB + RC//RD) ÷ RC//RD → RD = 474.3kΩ.

Using numbers from the example and substituting (Ra+Rb=92.8kohm = 92800ohm, and x = Rd):

2.45V=2.3V*(92800+((46400*x))/(x+46400))/((46400*x)/(x+46400))

plugging this formula into wolfram alpha to solve for x we get:

x = Rd = -47964

note that the answer in the datasheet is 474.3kohm

The answer I got would be close but it seems that the decimal place is off, if converter from 47964 to kilo-ohms it would be 47.964kohm which is 10 times less than the data sheet value.

Any help in determining what I did wrong would be great help! Thank you :)