Other Parts Discussed in Thread: TPS54331
Hi...
My requirement of power supply is
Type 1. input 24v Dc to 5V DC 3A +/- 2.5 % (Isotlated from input)
Type 2. input 24v DC to 5V DC 3A reg +/- 2.5%& 10v DC 300ma, reg +/- 10 to
15% (isolation between all o/p's)
Type 3. input 5v to 3.3v switching non isolating.
Can you suggest a suitable device that can cater to the above requirements?
I am not looking for a module. I am looking for a discrete part to design a solution.
Thanks
Suman G.