Please confirm an attached file.
Which is right information?
A. TPS6125xYFF D=1.206 +/-0.03mm
E=1.306 +/-0.03mm
B. TPS6125xYFF D=1.356mm(max),1.256(min)
E=1.256mm(max),1.156mm(min)
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Please confirm an attached file.
Which is right information?
A. TPS6125xYFF D=1.206 +/-0.03mm
E=1.306 +/-0.03mm
B. TPS6125xYFF D=1.356mm(max),1.256(min)
E=1.256mm(max),1.156mm(min)
The die size shown on page 26 is the correct one. Below dimensions are correct.
D:1.306 ±0.03 mm (Max =1.336 mm, Min=1.276 mm)
E:1.206 ±0.03 mm (Max = 1.236 mm, Min=1.176 mm)
Sorry for causing the confusion.
We'll update the datasheet accordingly