Hello,
I am working on an application that requires the switching control be regulated only based on input current or voltage, and I am currently investigating the possible use of the LM5118 for that application. Using the output voltage for control is not an option due to other independent power sources on the output bus. I am wondering if there is a way to reconfigure the vout sense and current sense pins to monitor and regulate the input current into the DC-DC converter to 14A.
Design specs are as follows:
Vin: 5-68V
I_in: 0-14A
I would be open to other IC's as well if someone has a better recommendation. Thanks in advance