My design uses the bq29410, which has a fixed threshold of 4.35V with a 4S pack. VDD is connected to the top of the cell stack, so max VDD is 17.4V.
What is the max voltage on the OUT pin? The datasheet shows a typical value of 7V with VDD=14V. Can it go as high as VDD?