This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS40140

Other Parts Discussed in Thread: TPS40140

Hello people.

I have a DC/DC aplication where the currente demand is very very high.

The minimum input voltage is 8V and maximum is 32V.

The maximum load charge is 4V at 60A.

I would use the TPS40140 in multiphase mode, however i have any doubts.

The TPS40140 part can work smoothly on a 5V power? The power stage will operate at 24V nominal.

  The base architecture is described in the page 57 of document below:

http://www.ti.com/lit/ds/symlink/tps40140.pdf

I can use this architecture or exist a best solution for my application.

Tanks.