Hello~
Connect the AC adapter to system, and then when testing the experiment for remove & mount of the battery (several times for short periods of time), sometimes charger status does not return to normal from battery fault.
It used almost fully charged battery products in the experiment.
In the general case, when remove the battery from system, FAULT bits of Status/Control register is setting to "111". And then, FAULT bits are returning to "000" after remounting the battery.
If the malfunction, FAULT bits does not go to "000" even if battery is remounting to the system. So, to solve this problem (to clear the FAULT bits), HZ_MODE bit has control (HZ mode enable --> HZ mode disable).
But this solution also has one problem, when HZ mode is active and the battery is removed, the system is turned off.
Even if Connect the battery, why does not clear the FAULT bit?? I want to know the reason.
In addition to controlling HZ_MODE bit, do you have another solution?
Does it have the minimum required time interval to remove the battery and connect it again?
I attached the schematic of BQ24168. Please check the schematic, too.
Thanks... C.W. :)