Hello,
i used Webbench to create a schematic for the LM3150 DCDC-converter. (The Webbench File and the schematic are attached.)
Input: 24Volt ; Output: ~7V / 1 - 10 Ampere variable
Now I got a problem with two boards. On this boards the Powerfet M1 (CSD17302Q5A) broken while power-on. The resistance of M1 is now less then 1Ohm an the output voltage = input voltage.
In the Power on moment the output current was less then 0.5Ampere.
After I replaced the Powerfet M1 the boards are working. But how long??
Do you have any ideas why the FET's are broken?
Thanks
Matthias
3302.WebenchReportsServlet.pdf