Looking through the manual for the TPS2511EVM-141 eval board, it appears that it is wired in Divider 2 mode(10W)? The datasheet for the TPS2511 shows how to wire it to Divider 1 mode(5W) by swapping D+ and D-.
There are jumpers to configure other features on the board, but are there jumpers to swap between Divider 1 and Divider 2 mode on the board? I don't see them in the schematic, but don't have an actual board in front of me yet to verify this.
If not, it sounds like I will need to do a little cut/jumper on the board. But just for out of curiosity, would the board work/charge an iPad at 1A in the Divider 2 mode if I set the current limit down to 1A?
Thanks,
Brad