Hi,
Has anyone had any experience of problems with the LM2731? I've used two in a new board that I'm working on. I'm feeding in 3.3V and have it configured for 5V output. I initially tried these unloaded, and then with a very light load (5mA). Both circuits (which are identical) just pass the input through to the output with no signs of switching occurring. I used the Webench designer to generate the circuit.
I did notice the following post, but other than requesting sending the IC's for investigation there is no outcome given.
http://e2e.ti.com/support/power_management/simple_switcher/f/858/p/183742/665559.aspx#665559
Thanks for any help.
Andy