I am using the 5 AC/DC portion of the PMP7389 design in one of my designs. I have found that my design stops providing 5 volts sometimes when a load is applied. The only way to get it back is to disconnect the input voltage for awhile and then reconnect. For debugging purposes I am using a 50 ohm resister to apply a load to the 5 Volts. Application of the 5 ohm resister does intermittently cause the power supply to stop. I have performed this test on the PMP7389 Eval board and have observed the same results. Is there something I can do to make this circuit less susceptible to loading and unloading??