This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
LM3410 is not working. I'm getting steady Vin (which is 5V) on pins 1, 4 and 5 and 0V on 2 and 3. It is not switching. It is frustrating because it should be very simple but it is just now working.
Right now I'm using an external source to supply 15-16V to LCD that is operating at 100mA although it can go up to 300mA. I'm just mentioning this to prove that LCD is working alright and over-voltage/open circuit protection may not be the case.
Picture is attached.
Please, any help / advice will be highly appreciated.
Thanks,
Ed
Hello Ed,
Have you checked all your connections and solderings so that there is not any cold solder joints?
Also if those are OK, have you replaced the LM3410 just to be safe?
Thank you,
Sami
Hi Sami,
Thanks for your response.
Yeah, I checked everything a few times. Now I'm waiting for evaluation board to compare. Hopefully I'll figure out what is going on.
Thanks,
Eduardo Garcia