Hi
I am using LMR62014 Boost regulator for 5v to 12v @100mA generation.
12v boost regulator output converted to 10v and 5v using PWM, using an RC filter followed by this generated voltages.
I faced some issues with this circuit.
- When I limited 5V input current below 200mA that time input voltage loaded. I can solve this problem when the input current to the regulator limited to 500mA. Both case there is no load connected. But after some continuous working that regulator failed. Now we lost two more regulators so please check this circuit and let us if we are missing something.