Hello!
I am prototyping with these two devices. As a reference I used QuickStartCalculator sheet, Evaluation Board documentation and datasheet - all available on the product pages at ti.com. My calculations, schematics, PCB layout and output waveform are all attached to this post.
Problem with LM5007MM: If I use SS16 diode (slow) everything is OK whatever load is applied. The problem arise if I use MURA110T3G diode (ultrafast) - the same diode is used in "AN-1298 LM5007 Evaluation Board User's Guide" and is suggested in datascheet "10V, 400mA Demo Board". With LED (5 mA) connected on the output the voltage is stable 5V. When resistive load of 134 Ohm is connected the output voltage gets unstable - its waveform attached below. The design makes audible noise whatever load is connected.
Problem witch LM5010MM: The same as with LM5007MM.
Why the design of LM5007MM made "according to the book" does not work for me? Why the problem appears if I use recommended diode type? Is the problem caused by incorrect properties of other component selected?
I appreciate any help or clue.