I have customer having the issue below. I need some suggestions on how to resolve this issue:
I have been chasing down a 150mV 16KHZ ripple on my 3.0V supply. The supply is sourced by a TPS62080A. My load is around 100mA. I found the problem was the snooze mode, disabling that dropped the ripple to <10mV. My question is at 100mA load, why is snooze mode kicking in? Or is that noise expected at any load?
Mode pin is pulled high when I see the problem. My understanding is by enabling it, it will only snooze when the load is light, which it is not right now. The load is light when the CPU goes to sleep (it currently is not in sleep) and so I wanted to have the snooze mode enabled because eventually the CPU will spend 99% of its time in sleep, so wanted better efficiency at light loads.