This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
I will use a PoE camera so I will use a LM3524D to build a power over ethernet injector, I built the Step-Up Boosted Current Configuration with the LM3524 and it works well (48v), but when I connect the camera (PoE, 80mA) the voltage is down and the circuit consuption is 7A , what do you recommend me to fix this issue