This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
From their datasheets the TLV61225 and the TPS61221 look nearly identical. Could someone please describe the differences between them, and what might make one better for a particular application than the other?
Thanks!
Hi Scott
the TPS device has better performance than the TLV device, such as the input voltage range (0.7~3.3V for TLV61225, 0.7~5.5V for TPS61221), and current limit accuracy (minimum Isw=160mA in TLV61225, minumum Isw=240mA in TPS61221, although typical values are the same).
if the customer need good performnce, they can choose TPS device. if customer need low cost , they can use TLV device.
thanks
jasper