Hello,
TPS2513 supports dedicated charging port Auto detect mode, DCP Divider 1(5 W) and Divider 2(10W). TPS2513A supports dedicated charging port Divider mode 3(12W).
My questions are:-
1) I have a 5V 5A transformer and if I select TPS2513A(12W) then it will draw 2.4A which is sufficient to charge one new I-pad. If I plug-in another I-pad, then both I-pads will be charged with 2.4 Amp or 1.2 Amp?
2) TPS2513A supports only Divider mode 3(12W). So is it possible to charge I-phone because I-phone charges with 5W charger or is it possible to charge i-pad (2.1A) which require 10W charger?
Any help in this is appreciated.
Thanks,
Chetan