Hi
I'm designing a mixed signal circuit board that shares its power rail with other circuit boards (third party designs). I would like to use a DC/DC switcher in my circuit to regulate the common +12V rail down to +3.3V for a microcontroller. I've been considering the TPS62173 (on the low end) and the TPS54120 (on the high end). However, I'm worried about noise being injected back on to the common +12V rail and hence affecting other circuits that are using it.
Other than using large input capacitors on the Vin of the DC/DC switcher, what else can I do to minimize the noise injected back on to the power rails? Is there a parameter in the datasheets of TI's DC/DC converters that is relevant here? Of course, an important consideration is the nature of the power supply that is providing the common +12V rail but let's assume that is also out of my control (for example, it could be a linear or switching supply).
Thank you!