We have an application for a bq77908A-protected pack that would use both maintenance (topping off the pack) and current taper limit (stop charge at 0.1C amps) chargers. Both charge and discharge protection FETs will be used, in series.
We're forced to have a two-pin pack only, no third charger detect pin would be available. We were going to set balancing to be on at all times but had a couple of questions.
- Is there a workaround to detect a charger being connected without a third pin on the pack? We can't think of one but was hoping TI might have some ideas.
- What would be the recommended method of connecting the CHGST pin if we're not detecting the charger? Pull up via resistor divider to PACK+/BATT+? Or better to pull up to VREG to minimize possible electrical noise or ESD on the pin, perhaps with a series resistor?
- The operating environment for these packs is extremely noisy (electrically). Do you recommend putting a small capacitor on the CHGST pin?