Hi All,
Would you mind if we ask BQ24031?
<Question>
Please refer to following attached file;
2626.Attached file.pdf
When the condition is the following, even though OUTPUT regulation volatage is 6.0V on the datasheet,
why does V-out of BQ24031 lower 4.4V?
Condition : BAT < 3.0V, TS=OFF, no-load
Does it have relation with BAT < 3.0V, TS=OFF and no-load?
Kind regards,
Hirotaka Matsumoto