This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24031 - TS=OFF with no-load

Other Parts Discussed in Thread: BQ24031

Hi All,

Would you mind if we ask BQ24031?

<Question>
Please refer to following attached file;
2626.Attached file.pdf

When the condition is the following, even though OUTPUT regulation volatage is 6.0V on the datasheet,  
why does V-out of BQ24031 lower 4.4V?
Condition : BAT < 3.0V, TS=OFF, no-load

Does it have relation with BAT < 3.0V, TS=OFF and no-load?

Kind regards,

Hirotaka Matsumoto