I made some area lighting by cascading three TLC5941s and using common-anode RGB leds. In order to produce more light in different directions, I connected 4 leds in parallel. I connected the common-anode to 5V, and connected all reds together, greens together, and blues together. Then the red went to one TLC5941 output pin, and green to another output, and blue to another output. The IREF pin is connected to a 1K resistor to ground, and my dot correction is set to 63 (39mA).
I have been having a few issues with leds not working all the time. For example, individually all R, G, and B work. But when I try to make yellow, one led is green but the other three are yellow - the red doesn't work for that particular led. I even had one led quit working altogether.
My question is, what is the proper way to connect CA RGB leds in parallel? Do I need to add a series resistor to each leg of each RGB led? Do I need to adjust the dot correction to different values for the red, green, and blue leds?