In my LiIon battery-powered application a TPS62203 is used to provide 3.3V. A TC54VC3002 supervisor disables the switch-mode regulator when crossing 3.0V.
Since the circuit draws around 120µA in stand-by, I was quite surprised to observe a jump in current draw upwards to >300µA. This observation would be correlated with a change from switch-mode to 100% duty cycle pass-through operation.
Such behaviour was observed in multiple circuits that may or may not contain ICs from the same batch (bought as T&R).
Is this a typical failure scenario due to thermal stress / ESD?