I am trying to determine whether a commercially designed battery charging product based on the BQ2954 is capable of operation using an input voltage other than that provided by the power supply provided.
The product currently uses a mains power supply at 12VDC +/- 0.5V and is designed to charge battery packs at 8.3VDC.at max 1A.
The design is based closely on the circuit given in the datasheet and uses scaling resistors RB1=310K / RB2=100K
I have an application where I want to power the charger from a vehicle supply using a 24V-13.6V Voltage Converter which has a worst case output range of 13.6V +15/-20% (10.88-15.64V).
I have carried out some basic tests substituting a bench power supply and varying the input voltage and found that although the circuit ceases to function below 11.2V (which I am not too worried about), the battery voltage was maintained within 0.1V for an increase in voltage to 16V.
I would be grateful for any advice on the factors that influence the line regulation that one might expect to achieve using a circuit such as the datasheet example.
In that example the input is marked as 8-24V +/- 10% - And the regulated battery voltage is stated at 4.2V - So one might assume that anywhere within this range is acceptable - So, in my application, would I be correct to believe that I can accommodate 12V-24? - But what is the significance of the +/- 10%? - Does this mean it could be 12V - 10% to 24V +10%?