This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
The Dim input control voltages at Vin at 5V are listed as:
Shutdown Threshold Voltage -- 0.4V
Enable Threshold Voltage -- 1.8V
If Vin is not at 5V, do these values change?
Also, what is the function of the 100k resistor attached to the DIM pin.
The datasheet list IDIM as 100 nA typ, Is this based on using the 100k resistor and does it change with Vin?
Ok I get that, but I still need this questions answered.
The Dim input control voltages at Vin at 5V are listed as:
Shutdown Threshold Voltage -- 0.4V
Enable Threshold Voltage -- 1.8V
If Vin is not at 5V, do these values change?
The datasheet list IDIM as 100 nA typ, Is this based on using the 100k resistor and does it change with Vin?