This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
We got a question from the customer about LM3410.
Could you help us?
[Question]
They are considering fast PWM dimming such as 20kHz(0~100%, 1% step) under the following condition. The IC has approximately 20usec delay time between rising edge of PWM signal and led current rising. Therefore they can't achieve this control. Are there any recommended schematics for their requirement?
Vin=3~5.5V
Vout=12V
Iled=120mA
They assume the PWM dimming circuit on figure 29 in datasheet might achive fast PWM dimming. Are there any concerns on this?
Best Regards,
tateo