This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
Yes, that is a valid way to analog dim with this device. I have not tried it but it is a common method used with many devices and most do not have startup issues with it. It is good to know that the LM3405 might in case I run into that issue.
Regards,
Clint
I could see that happening. It likely depends on all of the internal timing that you can't see in the block diagram. I'm sure some devices, if you have the current sense node already biased, may detect and overcurrent condition or something of that nature if it reads the current sense voltage while the internal reference is still not at full voltage. It is always best to test and always best to sequence just in case like you did with the LM3405. But many devices will have different timing and work just fine even if pre-biased.
Regards,
Clint