I'm using 8 PTH08T210W/PTH08T250W on a ATCA module to power Xilinx FPGAs with total power of ~300W. The datasheet of these DCDC modules require a minimum input capacitance of 470uF/1000uF. If I put one 1000uF Poly Alum capacitor in front of each DCDC module, the whole module will need 8 big capacitors and it takes a lot of PCB space. So the question is what is the minimum input capacitance of N PTH08T210W/PTH08T250W modules in parallel? Is that just N times the minimum capacitance of each PTH08T210W/PTH08T250W module? I hope it could be much less.