In the Diagram ,the source of high-side FET connect to BP7 seems error. Is the source connect to Vin.
I make a similar board to EVB, the out put is set to 1.8V. It do not not work when Vin below 7.4V.
Is the C15 in TPS53313EVM-078 can increase the voltage of BP7?
Hongxing Zhu, zhu@pcm.cn