Hi All,
One problem has been occurred on their test board which use UCC28070. Can you see below and give your advice? I can share their schematic by off line communication, so please email me directly.
[Situation]
- The drain current is limited at load transient from no load to 1.64kW at 90V input. This behavior is not confirmed at 95V input. (See Figure 1)
- This can not be resolved to increase RIMO and peak current limit threshold.•This behavior at 90V input can be resolved to change the bottom resistor at VINAC from 11kohm to 12kohm. (See Figure 2)
- However the ratio of divider value between VINAC and VSENSE can not be conformed if the bottom resistor at VINAC is changed to resolve it.
[Question]
- Please let me know the possible cause of this behavior.
- Please consider the solution to resolve this behavior instead of changing the bottom resistor at VINAC
Best Regards,
Sonoki / Japan Disty