A couple of the calculations on the TPS5405 datasheet are confusing me; either I'm going wrong somewhere (probable) or there is an error on datasheet.
Firstly, in equation (1): If I plug in 300kHz I get: 21.82 * 3e5^-1.167 = 8.85e-6. It should be around 8.55e4; where did I go wrong?
Now, Equation 3: In the example, what is the fsw meant to be!? this is not stated. I tried making fsw the subject to derive it;
fsw = (Vout / ( L / ( (Vin-Vout) / (Io * LIR) ) ) ) / Vin
using (from datasheet) Vout=5, Vin=12, Io=1, LIR=0.3 and L=5.4e-6; I get a value of 1800411.5.. or 1.8MHz
Is the 5.4uH result in the datasheet right? Or is my maths wrong?? 1.1MHz is listed as the maximum switching frequency (fsw). 180kHz would seem much more likely, which would require 54uH inductance.