This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
Are there the EMI test data of LM3409-Q1 ?
Also, can LM3409EVAL meet CISPR 25 Class 5?
Our customer will evaluate LM3409-Q1.
And they request the layout which can meet CISPR 25 Class 5.
If there are any improvement from LM3409EVAL for CISPR 25 Class5 please let me know.
I think that we can add the gate resister and snubber circuit.
<Specification>----------
Vin: 8V~16V
Vout:6~7V
Iled:0.7A~1A
-------------------------------
Best Regards,
Ryuji Asaka