Please check the attached schematic.
I like to make sure the components are correctly selected.
The data sheet is not clear on calculation Cadj (C0302 in schematic.)
can the ceramic caps be used for input and output caps?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Please check the attached schematic.
I like to make sure the components are correctly selected.
The data sheet is not clear on calculation Cadj (C0302 in schematic.)
can the ceramic caps be used for input and output caps?
Hello Stephen,
Your circuit looks good except that you should be using the TL317 instead of the LM317. Whenever I have used the "317" I have never been much concerned about noise - or I wouldn't be using the part - and so I have found that its operation is more than sufficient when not using the Cadj or the protection diode across the upper feedback resistor.
These parts are nearly unconditionally stable so I don't think you will have problems with your capacitor selection. But if you do have a problem with ripple try removing some of the ceramics first or add a cheap aluminum electric.
Bill