Hi,
I am currently working on a design with 6 TLC5941 onboard.
The system runs on 3.3V; SPI data and GSCLOCK comes from a PIC microcontroller. The 3.3V comes from a lineair voltage regulator that has 15V input.
This 15V input I also use to power my LEDs (strings of 5 white LEDs).
Everything runs pretty smooth, but something strange happens that I don't understand.
When I set the outputs of the TLC5941 to max (0xFFF PWM data), my voltage regulator gets very hot.
How is this possible?
The current that flows through the LEDs and the output transistors of the TLC comes from the 15V supply, not from the 3.3V supply.
Can somebody explain why my voltage regulator gets hot?
Thank you.
rene