We have used step down SMPS TPS54318 in one of our designs. The SMPS generates 1.2V output from input of 5V. The maximum load current at 1.2V is around 1A. Now we have a requirement where we need to remove all the devices from the board that use 1.2V supply. Thus there will not be any load current drawn from the SMPS. In this case what will be that state of the SMPS? Will be be shut off or the output voltage will still remain at 1.2V?
Note that we cannot remove the SMPS from the board.
Regards,
Elvin