This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Dual bq24725A. Need two chargers, two battery packs, single system.

Other Parts Discussed in Thread: BQ24725A, BQ24735EVM-710

Hello,


We are looking for a way to combine two BQ24725A chips to charge two battery packs (charge independently or both at the same time) and be able to use each battery separately.  We have bought/tested/familiarized with the eval board BQ24735EVM-710.  If we combine two designs based on this EVM, we can't control which battery discharges into the system voltage after the AC adapter is disconnected. 

Thanks!