Hi,
I am looking for a buck converter. And I notice LMZ21701.
I have some question as below.
1. As datasheet Page7 Figure 10. Radiated EMI on EVM==> For Radiated Emissions. Does it will be worse as this condition? Vin=9V and Vout=5V Iout=1A
2. I have 3 device need LMZ21701 to provide power. And the 3 device are separate in 3 area. Do I need to add bead in case of noise couple to other device?
3. For the GND. Doesn't it need to separate as PGND and AGND? Does it need to add more GND via for thermal and noise?
Please help to reply.
Thanks