This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I use LM2662 to transfer +5V to -5v
below is the input of LM2662
below is the output of LM2662
is it correct for LM2662?Or it‘s wrong design that causes the input be impacted?
Hello,
At what load current are the waveforms being taken at? The output ripple does look high and the input appears to me moving a bit. What is the resistance of L101? If this is high and the load current is high, you will see larger ripple.
If you power the LM2662 by itself using an external supply on the right hand side of the L101, does the ripple decrease?
Greg
hello,
1、the load current is about 80mA;
2、L101 is a bead, the resistance is 471Ω @ 100MHz; will the ripple smaller if the bead be removed?
3、power the LM2662 by itself using an external supply on the right hand side of the L101, the ripple at the input is lager , about 200mV, like below: