One of our customer is already using the LMZ14203H for a thermal printer application, the spec is
Vin min = 10.7V,
Vin max is 18V,
Vout = 9V
Iout = 2A, Peak is 5A
As the datasheet of this device mentions, that this device can support 5.4A peak current, could you please confirm whether this device can work for this specification/thermal printer application.