Hello,
Are there any suitable device for the following specification?
I think that LP8860-Q1, LM3431-Q1, LM3410-Q1 are similar with required specifications but not satisfied all requirement.
<Required Specification>
Vin : 3.3V or 5V (not fixed)
LED : 2S,1P
Vf : 3.3V (Vout=6.6V)
Iout : 400mA (device requirement is 500mA)
Dimming : Analog and PWM
PWM Dimming ratio : 1000:1
Best Regards,
Ryuji Asaka