This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC28700 NO LOAD REGULATION PROBLEM

Other Parts Discussed in Thread: UCC28700

Dear Sir,

I am using UCC28700 for my flyback converter application specs are 

Vinmin =300VDC,Vinmax =900VDC, Power=18 W, MOSFET used C2M1000170D silicon carbide MOSFET by CREE,problem which i am facing is durind NO load condition ie when larger loads like FAN,RELAYS,GPRS units are not turned ON .excessive ringing is found and the SMPS becomes unstable in some cases turns OFF .Flyback output voltages go above the required range at this condition for example 27V output goes to 36V at this no load condition.because of the above problem i was forced to keep the fan continuously ON so that NO load condition never exists.

Voltage divider RS1 is selected as 100K, and RS2 = 23k, Auxillary voltage feeding the controller is 24V .

Capacitor across VS terminal is removed, even oscilloscope probe contact to Vs pin can turn OFF the controller,which is also a problem and hence nothing can be measured across Vs PIN.

Rcs is selected as  1 ohm,Rlc=1K even though calculated value was 8K as u had given that higher resistance can be noisy,capacitor across CS pin is 10pF.

Gate resistor for the MOSFET is 62ohm, reducing it also did not help.

The primary inductance of the Flyback coupled inductor is 1.1mH, LEAKAGE inductance is about 60uH which is not very high.

It might be weird but when i touch the heasink of the MOSFET during no load condition it loses stability . TVS clamp is used to reduce the volatage spike across the primary.

Is it possible to solve the instability problem during NO load , and what might be the cause and how to rectify it.

As this project is at a very critical state i request you to help me in this.

 

  • Bharath,

    I will go through your values above against the datasheet equations to see if there any problems with the chosen design values. You have included a lot of detail, which is good.

    However, would it be possible to include a schematic?

    Also, can you confirm the transformer turns ratio Np:Ns:Na & the core cross-section (to calculate the Bmax)? And the value of the output capacitance (to see if there is enough for stable control loop).

    Have you included a pre-load or min load resistor at the output? This is always required with PSR to absorb the minimum power that would be transmitted at Fsw(min) - with the minimum output load, an OVP will happen for sure. In this case, the min power Pmin = 0.5*L*Imin^2*fmin = 0.5*1.1 m* (0.25/1)^2*1kHz = 34 mW - which is very low - it sounds like you are seeing issues well above this power level.

    It is recommended to put a scope probe at the top of RS1 (and scale the waveform) instead of putting a scope probe directly on VS, since the probe capacitance can affect the sampling.

    Is the heatsink floating? It would be better tied to primary local GND. It may be that the VS and /or CS pins are picking up noise, esp if touching the heatsink can make a difference.

    Can you also re-test with an electronic load on the output and confirm the load settings in W where the stability issues occur and go away? This will help us with debug.


    I will check the clacultations and revert with more suggestions when I get more details as requested above.

    Thanks,
    Bernard
  • Bharath,

    One more question for now, what was you design target Fmax? The UCC28700 can support up to 120 kHz, but what was your design target when calculating the inductance value?

    Thanks,
    Bernard
  • Dear Sir,
    105khz,maximum duty cycle is 0.47,Bsat of the core is 0.15Tesla inductance calculated is around 1.1mH.

    One more thing to add at 300V to 400V at NO load the smps turns ON and OFF frequently,if a load like a fan (1.8W) is present at that instant smps works wiithout any problems

  • Bharath,

    Here are some comments and notes from my review of your schematic and circuit values.

    1. I see that you have multiple outputs, on many different grounds. With PSR, the primary IC will regulate via the aux, so it will regulate whichever output is most heavily loaded. The other outputs may then increase in voltage, esp if they are very lightly loaded, depending on their individual leakage inductances.

    2. You mention that leakage inductance is 60 uH, how was this measured? Was it measured at the primary terminals (1-3) with all other windings shorted out? If so, then this will be a measure of all the leakages in parallel with each other, and could indicate much lower value than reality. I also think that 60 uH is actually not that small – it may seem so as a % of Lp, but at 100 kHz with Rcs = 1-ohm, the 0.5LI^2f power in the leakage would be 1.7 W. I would recommend that the leakage inductance should be measured at the primary pins 1-3, and note the value as each secondary is individually shorted, with all other secondaries open-cct. This will indicate the leakage from the primary to each individual secondary, which will be far more informative.

    3. In fact, since the ETD34 core is so large for this power level, and the turns are quite low (secondaries seem to all be in the range of 2T – 5T), it will be difficult to construct it with low leakage. I also think the Bpk is very low ~ 142 mT, the core is being hugely under-utilised. The transformer could be made much smaller by allowing Bpk to increase to ~300 mT.

    4. For my calculations, I follow the datasheet equations on pages 18-21. Assuming Dmax ~ 50% at min Vin (300 V), the max Nps is 12.6 (eqn 22) – you used 10, so that seems pretty reasonable. The primary reflected voltage will be ~ 277 V (assuming ~0.7 V Vf on D17). This will help to maximise the duty cycle, which will be good for eff. However, the snubber clamp zeners D18/19/22 may be a little tight to this (360 V Zener clamp), with such large leakage inductance, the clamp zeners may be getting quite warm.

    5. If the output power is 18 W total, the current limit should be set maybe 20% above this, maybe 22 W. Scaling all the other secondaries to the main 27.0VE output, this would indicate Iocc ~0.815 A. From eqn 23, Rcs should then be ~1.92 ohm. However, you used 1-ohm, indicating Iocc ~ 1.6 A, or ~43 W. Maybe this is necessary due to the characteristic of the fan loads at startup, but it does compromise the design, since would then be designed for 43-W max power capability, meaning the freq and duty cycle at 18 W would be much lower and less optimised.

    6. From eqn 25, assuming Fmax of 105 kHz, the required Lp value is calculated as 3.0 mH for Rcs = 1.92-ohm; or Lp = 1.6 mH for Rcs = 1-ohm. Since you use 1.1 mH, the controller will be forced to run at a higher freq, so it will hit it’s Fmax capability sooner than it will reach the 1.6 A Iocc, it will power limit early.

    7. Rs1 value looks ok, nominal start level will be ~270 V. It may need to be adjusted due to tolerance of Ivsl(run), if there a min Vin level where startup must be guaranteed.

    8. Rlc value depends on the turn-off delay. There is ~50 ns internal to the controller. Not sure how fast the SiC FET turns off. Let’s say about 250 ns total. With present values (1 mH & 1-ohm Rcs), Rlc should be about 6.8 k. With 1k value at present, the peak current will be bigger at higher input voltage, so more power can be taken, Iocc will increase with line, but so will Pmin. With the recommended values of 3 mH & 1.9 ohm Rcs, Rlc would be ~4.7 k.

    9. Finally, section 9.2.2.1 (page 18 of datasheet) verifies that the design can meet the Tonmin (actual Tonmin should be >300 ns) and Tdemagmin (should be > 1.1 us) constraints. With 1 mH & 1-ohm Rcs, Tonmin is 305 ns, this is tight to limit. But Tdemagmin is only 0.99 us, too short. This means that the PSR controller will struggle to regulate at min load because the Flyback interval will be too short for the internal circuits to arm and take a valid sample. This could be one of the causes of the issues seen here. With the recommended values of 3 mH & 1.9-ohm Rcs, Tonmin is 434 ns, Tdemagmin is 1.41 us, both ok with plenty margin.

    To conclude:

    - I think the combination of Lp & Rcs is not quite right for this power level.

    - For sure, the Lp & Rcs values will cause VS sampling and regulation issues at light load.

    - The ETD34 core seems very big for this power level, and Bpk of 142 mT is not fully utilising the core capability

    - The low turns count of the secondaries will make it difficult to minimise leakage inductance.

    - Multiple-output PSR designs will have cross-reg drawbacks, unless the load on all outputs is reduced together as much as possible, and there is a reasonable min load on each output when any of the outputs is heavily loaded. But this is due to the transformer construction and leakage inductances, it will also happen with opto feedback – except that opto feedback can be designed to favour one output, then the others will increase or droop depending on the cross-loading.

    - There may also be noise and layout issues to resolve, esp if you say that touching the heatsink causes issues. The drain node of the switch should be tracked as short as possible, with minimum possible copper trace area. I.e. Q1,R9/R70 & TR1 pin 3 all need to very close, connected together with a small short trace. This node has very high dv/dt and will radiate, so it's important to minimise the trace area. Similarly, the drain will capacitively couple to the heatsink, so the heatsink should be connected to local GND 0VSMPS node. The ferrite core of TR1 should also be grounded if possible using copper tape or wire that make good contact to the ferrite and then connect to TR1.6

    - Finally, the use of the SiC FET may also be significant. I think the UCC28700 should be able to drive that FET at 100 kHz, but the drain turn-off dv/dt may be much faster than with conventional MOSFETs, and this could also be causing noise issues.


    I hope this helps, let me know if you need any more information.

    Thanks,
    Bernard
  • Dear Sir,
    Thank you very much,all the suggestions given will be considered .

    Heat sink which was floating when connected to ground 0vsmps,the noload problem actually disappered ,smps is working properly without continous turn ON and turn OFF as before.
  • dear sir,

    the inductance when measured across the primary by shorting each output is given below

    27ve output when shorted = 276uH

    15ve output when shorted = 262uH

    18vspm output  when shorted= 380uH

    12vd output  when shorted= 440uH

    8vd output when shorted = 449uH

    24Vsmps output when shorted = 730uH

    I have a doubt whether the values are coupling inductances ???. because Aux winding and primary winding are right next to each other ,leakage inductance of 711uH is impossible.

    Note that i measured the inductance by keeping the RLC meter setting as series inductance .

  • Dear sir,

    the inductance when measured across the primary by shorting each output is given below ,this is for 1.1mH primary inductance
    27ve output when shorted = 276uH

    15ve output when shorted = 262uH

    18vspm output when shorted= 380uH

    12vd output when shorted= 440uH

    8vd output when shorted = 449uH

    24Vsmps output when shorted = 730uH

    I have a doubt whether the values are coupling inductances ???. because Aux winding and primary winding are right next to each other ,leakage inductance of 711uH is impossible.

    Note that i measured the inductance by keeping the RLC meter setting as series inductance .
  • Bharath,

    I see that you have attached many different transformer docs and design spreadsheets.

    Which are the correct or most up to date ones to look at? Which have you attached so many?


    To comment on your leakage inductance results, they do make sense. If you calculate the parallel equivalent of all of them, the result is 62.7 uH, which tallies with the 60 uH you reported when you first measured leakage inductance with all secondary windings simultaneously shorted.

    To illustrate why the leakage is so bad:
    - SWG30 = 0.315 mm Cu, so about 0.34 mm OD.
    - Primary is 60T, 60 x 0.34 = 20.4 mm. ETD34 bobbin width = 20.9 mm => 1 full layer.
    - For the 24Vsmps rail, this is 5T 1xSWG30. 5 x 0.34 = 1.7 mm => only fills 8% of layer width.
    - Due to only 8% overlap between prim and 24Vsmps windings, leakage will be very high.

    All windings are ideally multi-strand as many as possible, spread across the layer, to maximise area of overlap with primary, to minimise leakage. This is most important for the highest power windings in particular, take care of them first/closest to the primary, then add the less important aux windings.

    Note that the very large leakage on the 24Vsmps winding may be impacting the PSR regulation, even with C19 not populated there could be enough parasitic cap to give a significant LC filtering effect - if the waveform has no region of steady slope (i.e. too ringy or too softly rounded) the internal sampler may not get armed, the sample will be missed. it can happen that the IC repeatedly misses samples for several successive cycles, eventually leading to OVP. I would recommend using more starnds for the 24Vsmps rail to decrease its leakage, since it's used for the PSR sensing.

    Looking at some other leakages, the 18Vspm leakage is 380 uH, about half of the 24Vsmps rail, because it uses more strands and has slightly less turns. The 15Ve rail is 263 uH, the lowest, since it uses 8 strands for 3T, so total width is 3 x 8 x 0.34 = 8.2 mm. This has the widest width, so has the lowest leakage, but still is only ~40% overlap with the primary.

    Looking at your transformer spec, I also do not see any margin tape or triple-insulted wire being used, so how is the safety isolation provided for the isolated outputs?

    In your Excel sheets, you have made your own calculation that are different to recommended equations and method provided in the datasheet and in the TI design calculator.

    I would recommend to use the calculations that I previously provided, and modify your transformer construction for lower leakage inductance, esp on the winding used for PSR sensing. This should help improve your power supply performance.

    I would recommend liaising with a transformer vendor such as Wurth for advice and help to improve your transformer construction and implementation.

    Hope this helps.

    Thanks,
    Bernard