Not sure is this is the correct forum to post this query in so apologies in advance if not.
I need a 2.5V reference for my PIC 16F886 project to act as a voltage reference for the Analogue/Digital converters built into the chip. I found the LM385BZ2.5 which seems to fit the bill for price and spec on the datasheet but it only seems to want to produce 2.2V in my circuit rather than the 2.5V it should (2.425 to 2.575).
The reference is powered from a +5V regulated supply though a 2K5 resistor to the Cathode and the anode is connected to ground. This should give 1mA flowing through the device which operates from 20uA to 20mA. Thinking the PIC may be causing excessive loading, we added a op-amp voltage follower circuit which had no effect. The only thing that had any effect was a cap from cathode to ground which took the voltage up from around 2.16 to 2.2V.
Having followed the datasheet recommendations we are not really confused by this so any suggestion about what what we have done wrong will be gratefully received.
Bob