Dear valued community & TI experts
In my application of the TPS92074, an output voltage of 80V is needed. For the voltage sense circuitries on page 14 of the datasheet are only avaiable up to 65V LED stack voltage. The alternate method bridge tap is suggested - where can I find additional information about this? Or are there other possible VSEN circuit options?
In the application notes a converter with 75Vout is described using a similar VSEN circuit as the one suggested in Figure 14. of the datasheet.
Please note, that the input voltage in our application is at 230Vac.
Thank you
Sam