This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PMP9444 - replacement the TPS40428 with the LMZ31710 and modification of the XML files for Fusion Digital Power Designer

Other Parts Discussed in Thread: PMP9444, LMZ31710, TPS40428, UCD90120A

Dear team, 

One of our customers ( Avnet EMG, CERN) has the following questions about the reference design PMP9444.

http://www.ti.com/tool/PMP9444?keyMatch=PMP9444&tisearch=Search-EN-Everything

"

1. Where I can find XML files for Fusion Digital Power Designer for PMP9444?

2. I would like to use my board in system with 5V backplane but also 12V backplane and for VCCINT I need max. 10 A. It is possible to modify power solution for Kintex-7 Ultrascale FPGA in such way that Vin can be in range 4.5 -12.5 V? According to requirement VCCINT= max.10A , can I replace TPS40428 + 2x CDS95378 by LMZ31710 and such achieve range for Vin 4.5-12.5 V ?

3.  Can you advice how to modify XML files for this replacement?

"

About the first question, I found on the forum the files that I have also enclosed to this post.

Could you please advice for the other questions?

Thank you very much for your support.

Best regards,

 

Massimiliano De Cristofaro

Application Support Engineer - Power Management

ASKTEXAS DiamondLane – EMEA Distribution Support

Texas Instruments Deutschland

5314.UCD90120A.zip