When in negative mode, what are the requirements for Vin?
For example, is it possible to get Vout: -15VDC from Vin: 12VDC
and
For example, is it possible to get Vout: -5VDC from Vin: 12VDC
Also in this case what would be the current rating compared to normal operation?
Is there a minimum voltage difference required like the case for possitive operation?
Vin should be Vout +3VDC