This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMZ14203H

Other Parts Discussed in Thread: LMZ14203H

When in negative mode, what are the requirements for Vin?

For example, is it possible to get  Vout: -15VDC from Vin: 12VDC

and

For example, is it possible to get  Vout: -5VDC from Vin: 12VDC

Also in this case what would be the current rating compared to normal operation?

Is there a minimum voltage difference required like the case for possitive operation?

Vin should be Vout +3VDC