Hi,
I have designed a 27VDC/3.3VDC PS. It appears to be working correctly but after having a closer look the output voltage does not look clean, which in turn appears to create problems in other parts of the circuit. Originally I designed it using Webench for 100mA, but the actual load ended up being ~30mA (with short 6ms bursts of additional ~20mA). I tried running it in the DCM as well. But the ringing is still there.
Any suggestions welcome.
Thanks