What is the difference between a POE Adapter and POE Midspan Injector? Are both the same?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
What is the difference between a POE Adapter and POE Midspan Injector? Are both the same?
Hi Darwin,
Thanks for the response.
Then can you pls let me know if the below 2 datasheets are for the similar products, the difference being only in their power ranges?
Since one is an injector and the other is an adapter
Hi Gaayathri,
From these two datasheets, we can see that they apply same function for different power ranges.
They use different terminologies to indicate an injector, either PoE Midspan or PoE Adapter.
There is no clarified statement to explain which one is correct; however, their application are the same as shown in Fig. 1 A.
Otherwise, there is another device is PoE Splitter. In Fig.1 B, we can use a PoE injecter to connect with a PoE Splitter for powering an non-PoE device.
Fig.1