Hi,
Can TPS51220 or TPS51220A, TPS51221 be used to implement 2-phase, single output buck converter?
Thank you,
John
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
None of these devices can be used for single output converter
Regards
Mike
Hi John,
I don't agree with you.
if you connect COMP1 and COMP2 together, how will you connect VFB1 and VFB2? also connect together to the single feedback?
you know the two error amp of two channels will not have same input offset, which means if one error amp think VFB is regulated, and another amp must think VFB is not regulated yet, this will cause problem.
you can try if you insist your method works
regards
Mike